Showing results for 
Search instead for 
Do you mean 
Reply

Edit name of NX

How i can edit the name of NX , 
123.png

14 REPLIES

Re: Edit name of NX

You can control what is displayed in the NX title bar with the "TITLE" command in Menuscript. For example:

VERSION 120

EDIT UG_GATEWAY_MAIN_MENUBAR

TITLE ** NX ROCKS **

Save it as "MyTitleBar.men". You can name it anything, but the extension must be ".men". The important thing is that this file must be located in a folder that NX will find while it is starting up.

The .men file must live in a folder named "startup". This folder should be located immediately UNDER any directory defined by UGII_USER_DIR, UGII_VENDOR_DIR or UGII_SITE_DIR. You can also put the "startup" folder immediately UNDER any folder mentioned in your custom_dirs.dat file.

So for example, having defined UGII_USER_DIR to point to "C:\user_dir". Place a "startup" folder under that directory, and the .men file is: C:\user_dir\startup\MyTitleBar.men

Regards, Ben

Re: Edit name of NX

where i can find "TITLE" command in Menuscript ? Please tell me detail !

Re: Edit name of NX

Re: Edit name of NX

Hello Experts,

 

as per benbroad told i done that but cant change Titlebar,,

 

 

help us if u can!!!!!!!!!

 

also seen in help, but cant understood

 

can somebody upload short movie video for it guys!!!!!!

 

 

 

 

 

 

 

 

Best Regards
Thomas Roman
Machine Designer

Re: Edit name of NX

Hi Thomas,

Try this.

Create a custom folder and then use this Env Variable UGII_USER_DIR to point to it. Then inside the custom folder create a startup folder and paste the attached .men file inside it. You should see SiemensNX (change it in the men file to show whatever you want to display)rather than showing the version next time you launch NX.

Please rename the extension of the file attached to .men 

Regards

Kapil

 

 

Re: Edit name of NX

THanks@kapilsharma for help ,,,

 

 

i wanna ask another crazy question

 

How i can customize or edit NX & SIEMENS logo

 

have anybody got  idea for this

 

 

 

Capture_Logo.JPG

 

 

Best Regards
Thomas Roman
Machine Designer

Re: Edit name of NX

Smiley Happy   absolutely no idea Thomas. I am not sure if it can be done using .men file .

Regards

Kapil

Re: Edit name of NX

anybody else guys 

 

if another have some idea share it guys

 

 

 

 

 

Best Regards
Thomas Roman
Machine Designer

Re: Edit name of NX

I've got to ask.. why?

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | C# | KF
Production: NX8.5.3.3 MP11 64bit Testing: NX9.0.2.5