Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

Error in NX default Schema (Mechanical Routing)

There is an error in NX default schema used to import run. As, when I try to import runs using the nx default example (smaplepiperun.xml), I am getting error that Cant read the attached xml file, check that correct schema is used.
9 REPLIES

Re: Error in NX default Schema (Mechanical Routing)

I ATTACHED THE FILE ( smaplepiperuns.xml) for your review.

Re: Error in NX default Schema (Mechanical Routing)

Hi,

I could not find any attachment.

Best Regards

Kapil

Re: Error in NX default Schema (Mechanical Routing)

 

Re: Error in NX default Schema (Mechanical Routing)

I am browsing it, however it is not showing !

Re: Error in NX default Schema (Mechanical Routing)

Solution
Solution
Accepted by topic author mona_hegazi
‎11-11-2016 05:21 AM

Re: Error in NX default Schema (Mechanical Routing)

Download the attached file; SamplePipeRuns.txt, and rename the file extension to .xml.  Place it in a directory with a copy of your PipeRuns.xsd (schema) and choose Import Runs.  It should work now.  There was an unrecognized attribute and a value missing.

 

Regards, Ben

Re: Error in NX default Schema (Mechanical Routing)

Yah it worked, thank you. However, the parts are missing. Import run are not importing the assembly parts as well yes ???

Re: Error in NX default Schema (Mechanical Routing)

 

Re: Error in NX default Schema (Mechanical Routing)

I UPLOADED A screenshot from the run navigator for your kind review after I import it, however not all I can not have an active parts, is this correct ? https://drive.google.com/drive/folders/0ByQZFzXbN-jGRW1LOXRoRElGb3M