Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

How to Edit Properties en masse? NX 9

I'm looking  for a method to edit properties en masse.  I am new to NX but a long time Solid Edge User.  In Solid Edge there is a tool call "Property Manager".  From there we can edit all associated files from an assembly or from a directory.

 

What is the best approach to Mass Edit properties in NX?  Either via the UI or ever at the OS level.

 

In NX 9,  from an assembly I have found group select, properties, bulk edit...  but this appears to limit the properties to edit down to the least common shared Props...?

 

TIA!!!

 

Matt Johnson

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8) (SEEC)
Teamcenter
NX9
9 REPLIES

Re: How to Edit Properties en masse? NX 9

I'm wondering if you can push updates down via the spreadsheet functions? Open the spreadsheet, import attributes and then push them down the assembly structure.

Maybe Taylor Anderson will pipe in....

Re: How to Edit Properties en masse? NX 9

Matt-
Welcome to NX. It's a much freer world here..which is a double edge sword.

Re: How to Edit Properties en masse? NX 9

unfortunately I have a installed versions mismatch. I have Excel 2013 installed and running NX9... I believe Excel 2013 is not supported until NX10. We will be upgrading to NX10... I will investigate more at that time.

thanks for you input!
===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8) (SEEC)
Teamcenter
NX9

Re: How to Edit Properties en masse? NX 9

Even though your Excel version may not be "officially supported", it will still probably work with NX 9.

 

I'm not an SE user, but from your description, it sounds like SE offers more options for "bulk editing" than NX does. One option would be to write some custom code to import/add your desired attributes. I'd be glad to help with that if you post or PM some details such as what form your attribute/value list is currently in (text file, spreadsheet, existing part, etc), what to do if the attribute already exists (keep current value, overwrite with new value, etc), what type of report (if any) to give for processed parts, etc etc.

Re: How to Edit Properties en masse? NX 9

Thank you much for the offer.

When I try to launch Spreadsheet it just seems to hang with a status bar message of "Transferring Control to the Spreadsheet..." but just hangs there...

I don't really have a need to write Attributes at this time... I'm trying to test Importing to Teamcenter and actually need to delete some attributes because I'm having some LOV conflicts...



===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8) (SEEC)
Teamcenter
NX9

Re: How to Edit Properties en masse? NX 9

Do you only need to delete part attributes or are you looking to delete other attributes as well (component attributes, feature attributes, body attributes, etc)?

Re: How to Edit Properties en masse? NX 9

part attributes... in my case "PG_PART_TYPE"
===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8) (SEEC)
Teamcenter
NX9
Solution
Solution
Accepted by topic author MattJohnson_PG
‎09-08-2016 07:26 AM

Re: How to Edit Properties en masse? NX 9

[ Edited ]

Here's a quick journal that when run will prompt you to select a directory; it will then process all the part files in the directory and attempt to delete the "PG_PART_TYPE" attribute. It isn't heavily tested, I suggest copying several of your files to a new directory for testing, and creating backups of the files that you intend to use it on. It does not check to see if anything else references the attribute before attempting to delete it (such as drafting notes, expressions, or other attributes). It tries to save the file after deleting the attribute, so you will need write access to the folder/files. In its current state, it only processes the folder specified, not any of its subfolders. If desired, you can process subdirectories by passing "True" as the second argument to the "processParts" subroutine.

 

'Journal to Cycle All Part Files in a specified folder (with option to include subfolders)
'based on 'cyclePartFiles' code example from GTAC
'
'This journal will prompt for a folder (selection dialog)
'then open each file, delete the specified part attribute, and then save & close the file.



Option Strict Off
Imports System
Imports System.IO
Imports System.Collections
Imports System.Windows.Forms

Imports NXOpen
Imports NXOpenUI
Imports NXOpen.UF

Module attribute_deleter
    Dim theSession As Session = Session.GetSession
    Dim LW As ListingWindow = theSession.ListingWindow

    Dim workPart As Part = theSession.Parts.Work
    Dim displayPart As Part = theSession.Parts.Display
    Dim initialPart As Part = theSession.Parts.Display

    Dim nTotalPartFiles As Integer = 0

    Sub Main()

        Dim strOutputFolder As String
        LW.Open()

        Dim FolderBrowserDialog1 As New FolderBrowserDialog
        ' Change the .SelectedPath property to the default location
        With FolderBrowserDialog1
            ' Desktop is the root folder in the dialog.
            .RootFolder = Environment.SpecialFolder.Desktop
            ' Change the following line to default to a given path
            .SelectedPath = "C:\"
            ' Prompt the user with a custom message.
            .Description = "Select the directory to scan"
            If .ShowDialog = DialogResult.OK Then
                ' Display the selected folder if the user clicked on the OK button.
                'msgbox(.SelectedPath)
                strOutputFolder = .SelectedPath
            Else
                'user pressed "cancel", exit the journal
                Exit Sub
            End If
        End With

        LW.WriteLine("Cycle All Parts in a Folder Tree")
        LW.WriteLine("Start Time: " & CType(TimeOfDay(), String))
        LW.WriteLine("")

        Try

            processParts(strOutputFolder, False)

        Catch ex As NXException
            LW.WriteLine("Cycle Files and Folders Error: " & ex.Message)
            Exit Sub
        End Try

        LW.WriteLine("")
        LW.WriteLine("Number of part files processed: " & nTotalPartFiles)
        LW.WriteLine("Stop Time: " & CType(TimeOfDay(), String))

    End Sub


    Sub processParts(ByVal directoryPath As String, ByVal includeSubDirs As Boolean)

        'Process All Parts in a specified directory

        Dim nPartFiles As Integer = 0
        Dim part1 As Part = Nothing
        Dim files() As String
        'save the current load options
        Dim curComponentLoadOption As LoadOptions.LoadComponents = theSession.Parts.LoadOptions.ComponentsToLoad
        'set load option to NOT load components
        theSession.Parts.LoadOptions.ComponentsToLoad = LoadOptions.LoadComponents.None

        If includeSubDirs Then
            files = Directory.GetFiles(directoryPath, "*.prt", SearchOption.AllDirectories)
        Else
            files = Directory.GetFiles(directoryPath, "*.prt", SearchOption.TopDirectoryOnly)
        End If
        For Each fileName As String In files
            nPartFiles += 1
            nTotalPartFiles += 1
            LW.WriteLine("  " & Path.GetFileName(fileName))

            If (IsNothing(initialPart)) OrElse (initialPart.FullPath <> fileName) Then
                Try
                    part1 = theSession.Parts.OpenDisplay(fileName, Nothing)
                Catch ex As NXException
                    LW.WriteLine("open error: " & ex.Message)
                Catch ex2 As Exception
                    LW.WriteLine("exception: " & ex2.Message)
                End Try
            Else
                'LW.WriteLine("initial part equals display part: " & initialPart.Equals(displayPart).ToString)
                part1 = displayPart
            End If

            displayPart = theSession.Parts.Display
            workPart = theSession.Parts.Display

            'do something
            'write your own subroutines and/or functions to process the part and call them from here
            DeleteAttribute("PG_PART_TYPE")

            'save file
            Dim partSaveStatus1 As PartSaveStatus
            partSaveStatus1 = part1.Save(BasePart.SaveComponents.False, BasePart.CloseAfterSave.False)
            partSaveStatus1.Dispose()

            'close file unless this file was initially open
            If (IsNothing(initialPart)) OrElse (initialPart.FullPath <> fileName) Then
                part1.Close(BasePart.CloseWholeTree.True, BasePart.CloseModified.CloseModified, Nothing)
                part1 = Nothing
                workPart = Nothing
                displayPart = Nothing
            End If

            If Not IsNothing(initialPart) Then
                Dim partLoadStatus1 As PartLoadStatus = Nothing
                Dim status1 As PartCollection.SdpsStatus
                status1 = theSession.Parts.SetDisplay(initialPart, False, False, partLoadStatus1)

                displayPart = theSession.Parts.Display
                partLoadStatus1.Dispose()
                theSession.Parts.SetWork(displayPart)
                workPart = theSession.Parts.Work
            End If

        Next fileName

        'reset load option
        theSession.Parts.LoadOptions.ComponentsToLoad = curComponentLoadOption

    End Sub

    Sub DeleteAttribute(ByVal attributeTitle As String)

        'delete the specified attribute from the work part

        If theSession.Parts.Work.HasUserAttribute(attributeTitle, NXObject.AttributeType.Any, -1) Then

            Dim markId1 As Session.UndoMarkId
            markId1 = theSession.SetUndoMark(Session.MarkVisibility.Visible, "delete attribute")

            Dim objects1(0) As NXObject
            objects1(0) = theSession.Parts.Work

            Dim attributePropertiesBuilder1 As AttributePropertiesBuilder
            attributePropertiesBuilder1 = theSession.AttributeManager.CreateAttributePropertiesBuilder(theSession.Parts.Work, objects1, AttributePropertiesBuilder.OperationType.None)

            attributePropertiesBuilder1.Title = attributeTitle

            attributePropertiesBuilder1.Delete(theSession.Parts.Work)

            attributePropertiesBuilder1.Title = ""

            Dim nXObject1 As NXObject
            nXObject1 = attributePropertiesBuilder1.Commit()

            Dim id1 As Session.UndoMarkId
            id1 = theSession.GetNewestUndoMark(Session.MarkVisibility.Visible)

            Dim nErrs1 As Integer
            nErrs1 = theSession.UpdateManager.DoUpdate(id1)

            attributePropertiesBuilder1.Destroy()

        End If

    End Sub

    Public Function GetUnloadOption(ByVal dummy As String) As Integer

        'Unloads the image when the NX session terminates
        GetUnloadOption = NXOpen.Session.LibraryUnloadOption.AtTermination

    End Function

End Module

 

Copy the code above to a text file (use a plain text editor such as Notepad) and save it to a convenient location; be sure to change the file extension from .txt to .vb. To run the journal, go to menu -> tools -> journal -> play... and select the journal file then press the "run" button. This journal does not require you to open a part before running it; and it may actually work better if you don't have any open parts before running it.

Re: How to Edit Properties en masse? NX 9

@cowski1,   thank you very much!

 

Sincerly appreciate your time and effort!!!

 

Above and beyond!

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8) (SEEC)
Teamcenter
NX9