Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

How to create a circular spring in NX9

Hello,

 

Any help for creating a circular spring? Enclose a photo

 

Outer diameter Spring: 3 mm

Wire diameter: 0.4 mm

Length circumference: 247 mm

 

Thanks

 

Jose C

 

3 REPLIES
Solution
Solution
Accepted by topic author JCP
‎10-21-2016 07:24 AM

Re: How to create a circular spring in NX9

Hello,

you can use law curve and tube. 

 

Example part is attached. There is necessary edit some parameters.

 

Marek S.

Re: How to create a circular spring in NX9

Hello,

Thanks for your example.

have a good day

Jose C.

Re: How to create a circular spring in NX9

Also in addition to that part, NX provides examples for law curves in the reuse library samples that everyone gets.In addition to other kinds of objects. 

 

Sample Reuse Included with NXSample Reuse Included with NX

 

Scott