Showing results for 
Search instead for 
Do you mean 
Reply

Loaded Assembly but no assembly tools

I have loaded an assembly but it has opened as if it is in modelling, with none of the add component tools etc, usually seen in the assembly window, available. Can anyone help solve this?

1 REPLY

Re: Loaded Assembly but no assembly tools

Sounds like the assemblies application is not on. Try under File (start) click and switch on Assemblies .  Alternatively in the Applications tab click the assemblies button.

 

You may also need to right mouse click at the end of the ribbon bar and switch on the Assemblies tab.

Steve V