Showing results for 
Search instead for 
Do you mean 
Reply
Solved! Go to solution

NX10/11 Part Copy Method - Reusable Component

This customer default was added in NX10 for Resuable Component under Gateway, but I don't understand what the intent is, the description in the what's new doc doesn't really describe it very well.  What's this for?

 

PartCopyMethod.PNG

2 REPLIES
Solution
Solution
Accepted by topic author elopategui
‎11-10-2016 06:31 PM

Re: NX10/11 Part Copy Method - Reusable Component

In the Reuse Library, the Part Copy Method option is used to determine how to create a copy on the template part.

 

  • “Use Clone Assembly” equals NX Clone (Assemblies > Cloning > Create Clone Assembly) which will create the copy right away in the native file system or the Teamcenter database.
  • “Use Part Rename” loads the part first and then uses NX part rename.  The advantage is that the user can discard the result by not saving it.  It’s faster than the other 2 methods because the saving has not already started.
  • “Save As”  - Loads the part first and then uses the same functionality as "File > Save As" which will create a copy always as the first option.

Prior to NX 10, the part copy method used the “Use Part Rename” method.  The other methods were not available in the customer defaults.

 

Does that help?

Regards, Ben

Re: NX10/11 Part Copy Method - Reusable Component

Thanks Ben that was exactly what I was looking for!