Reply

After entering activation code status bar loads for days but doesnt complete

I downloaded the 45 day free trial of Solid Edge ST7 a few days ago and when I enter my activation code the status bar that shows its loading and processing my activation continues to load forever but doesn't complete. I left it running to load for 3 days and it still did nothing except say it was processing my activation and that it should only take a few minutes. I am a student and I have work to do. I really need help as soon as possible and any help is greatly appreciated.

1 REPLY

Re: After entering activation code status bar loads for days but doesnt complete

Hi there,

 

"3 DAYS", Yikes!!!...no way I'd have waited longer than 3 minutes, and thats being rather generous for the action being performed. This type of problem points to a corrupt installation file, or incompatible system.

 

If you're a student....why not download the free "Student Edition"?

 

 

 

Aslo to note....Solid Edge ST7 is the first release that is ONLY coded for use in 64bit Windows.

[stay on ST6 if you have a 32bit installation of Windows]

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10