Reply

Hole wizard

Is it just me or is the hole wizard not included in this trial version.
I'm trying the tutorial and simply can not get the hole icon in the solids section to work. This make it very difficult to gain anything from the tutorial.
3 REPLIES

Re: Hole wizard

It is included. When you select the Hole command, in the command bar that appears at the top of the graphics window, click the Hole Options button.
Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Hole wizard

No, in the command bar "Home" for solids the "Hole", "Draft" and "Thin wall" as well as the what is in their drag down is "gray'ed" out.
I tried several tutorials but I get stuck when I can't use these features.
Is this a set-up problem ?

Re: Hole wizard

Perhaps post a picture. Did you have another Solid Edge product loaded like Solid Edge 2D Free?
Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1