Reply

Solid Edge Web installer ST7 disappears/shuts down after accepting the terms of agreement

 

This is actually the last Window I see from the web installer (45 day trial).

The installation doesn't start at all.

 

Client is a standard Win7 64bit SAG gain client.

 

Reboot was done, still no difference.

English and German LP tested, same result.

 

Has anybody a solution to this?

 

BR
MartinF

 

 

2 REPLIES

Re: Solid Edge Web installer ST7 disappears/shuts down after accepting the terms of agreement

First question - can you write to the C: drive?
Second question - what is " Win7 64bit SAG gain client"?
Cheers
Mark

Re: Solid Edge Web installer ST7 disappears/shuts down after accepting the terms of agreement

Hi Mark,

 

thanks for your promt answer.

First: It's a standard Siemens client within the network. So main difference would be:

- policy controlled access rights to c:\root where the webinstaller wants to save the installation files

c:\SEV107WebInstall

 

This can be solved by starting the webinstaller directly as local administrator.

 

I guess it can't use the system proxy, so the connection to download the files can't be established.

 

This was solved by downloading the files on a 'private' client without proxy.

 

Installation on the Siemens client worked by coping them.

 

Now I got the next issue about the proxy, I can't activate the trial Smiley Sad

 

Is there a possibility to configure Solid Edge to use the system proxy?

 

Thanks in advance!
Martin