Reply
Solved! Go to solution

2D ST7 - Dimensions don't rotate with attached objects

I'm just an occasional user of the 2D version.

 

If I rotate, for example, a rectangle including the dimensions for length and width, the dimensions do not rotate, the horizontal dimension stays horizontal while the line it is attached to is now vertical, and the vertical dimension stays vertical while the line it is attached to is now horizontal, and so both dimensions now have values of zero.

2 REPLIES
Solution
Solution
Accepted by topic author Tige
‎08-26-2015 04:32 AM

Re: 2D ST7 - Dimensions don't rotate with attached objects

Hi there,

 

This is the nature of the dimension orientation style "Horizontal/Vertical" applied.....had you used either of the 2 others, then they would follow the geometry when rotated.

 

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: 2D ST7 - Dimensions don't rotate with attached objects

Thank you. That does the trick. This setting is not in the properties dialog.