Reply
Solved! Go to solution

Assembly JT import as .par

Hi Edger´s

 

I want to Import an Assembly JT into a .par Template.

 

But unfortenately the result is an teselated Body feature...

 

In my opinion i should get an multibody Part with two Volume bodys...

 

What am i doing wrong?

 

The funny thing is, if i open this jt with an .asm template i get an .ASM with two parts and they are correct as expected.

 

I also tried some settings in the SePvTrn.ini, "Import Multiple Bodies As Single Part file=On" but for me there was no change in the results...ASM TemplateASM TemplatePAR TemplatePAR Template

 

Thanks in advance, see attached the Jt file (I had to ZIP it because .JT is not allowed as attachement...)

 

 

6 REPLIES

Betreff: Assembly JT import as .par

[ Edited ]

Hi,

 

 

 

could it be, that You only exported a rough (triangle)  JT file instead of a fine (B-Spline) .

That could explain the teselated body.

 

There is an option in the export steps to define the quality of export.

 

 



regards
Wolfgang

Betreff: Assembly JT import as .par

Hi,

 

yes i know that options, i used the settings ses screenshot (iclude precise geometry)

JT OptionsJT Options

 

See also my comment in above with the .ASM template.....

 

 

Betreff: Assembly JT import as .par

Hi,



OK, it seems, that the JT is a fine geometry rather then a coarse.

Importing the JT file into an assembly creates a parts structure which also could be modified.

 

 

At the moment I only see a way to import the asm first and interpart that into a part document.

 



regards
Wolfgang

Betreff: Assembly JT import as .par

Thanks for the answer,

 

I also tried this before, it works correct, but i just do not understand this behaviour...

 

We have implemented the Multibody technique, so why this is not working on JT Import.

 

Greetings Christian

 

 

Betreff: Assembly JT import as .par

Hi,

maybe it is a matter of the translator rather then Solid Edge itself.


regards
Wolfgang
Solution
Solution
Accepted by topic author c_weber
‎11-02-2016 05:03 AM

Betreff: Assembly JT import as .par

Hello together,

 

i filed an IR, it  was an PR and now it is an ER 867196 with the status OPEN

 

Just for your information, if you have the same Usecase.

 

Regards Christian