Reply

CAMWorks for ST9

For any CAMWorks users out there, I have word that the update that allows it to work with ST9 is coming out in about 4 weeks. In my experience that means 4 weeks minimum, but they are working on it.

 

Larry K

4 REPLIES

Re: CAMWorks for ST9

larry

 

Thanks for checking. I have just nicely got into camworks and was wondering when I would be able to update to st9.

 

Regards,

 

Duane M

Re: CAMWorks for ST9

CAMWorks SP3 is available for download today. I haven't tried it out yet. Remember to back up your custom TechDB and anything else before installing.

 

Larry

Re: CAMWorks for ST9

Thanks larry

Re: CAMWorks for ST9

Also, I think it is better to upgrade CAMWorks first and make sure it is working and then upgrade Solid Edge. It's worked well for me in the past.