Reply

Can't open file. not correct version?????????????

Morning all

I have this file i open yesterday with out a problem. now i can not open it. please help say's i can't, please help

7 REPLIES

Re: Can't open file. not correct version?????????????

by the way it's now two files. i also just updated to 9 the other day.

Re: Can't open file. not correct version?????????????

I think you need to contact your VAR or GTAC.  Not sure anyone here can help as it sounds like a corrupt file or a bug.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Can't open file. not correct version?????????????

Yea, i'll call in monday

Re: Can't open file. not correct version?????????????

Normally you would see this message when you are trying to open files that were created with a newer version of Solid Edge.. Since you are using ST6 could it be that you have received files from someone thats using ST7 (beta) ?

 

Re: Can't open file. not correct version?????????????

nop, these files were created by me myself and i. reminds me, do need to call these in

Re: Can't open file. not correct version?????????????

[ Edited ]

Any chance that anyone has accessed the affected files with Solid Edge Student Edition?....as this would kill the files off from being used by any commecial version, and give that very message.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Can't open file. not correct version?????????????

I have the same problem. Strangely the problem occurred on several workstations after installing MP8. The problem observed for at least 30 files, looking for some dependencies, and it happened to me this implies that the opening of a single file by multiple users, but I do not know because it's hard for me to replicate this error. Equally Yesterday I had a similar case.
SE ST8 + TC 10.1