Reply
Solved! Go to solution

Capture Fit auto-set

My ST7 would identify how a part was mated in an assembly, and I didn't have to set capture fit for that part. Where is the setting to turn that on? Now that I'm on ST8, I have to set capture fit, for SE to remember how I located a part.

ST8 MP9
Go FAST, or go home.
3 REPLIES

Re: Capture Fit auto-set

[ Edited ]

There is an option you can set in the Assemble Options that will automatically capture them during placement. Maybe you had that set in ST7?

 

autocapture.png

 

Greg

Re: Capture Fit auto-set

I have yet to find that setting, looking in the assembly settings.

ST8 MP9
Go FAST, or go home.
Solution
Solution
Accepted by topic author BoatTech
‎04-18-2016 07:36 AM

Re: Capture Fit auto-set

[ Edited ]

It's not in Solid Edge Options, it's in the Assemble command. Click on the 'Options' button on the Assemble Command Bar:

 

assembleoptions.png

 

That button will bring up the dialog I posted above. Some of these options are also available in Solid Edge Options, but not all of them.

 

Hope this helps,

Greg