Reply

Convert ST2 drawing to ST5

[ Edited ]

I open ST2 draft file in ST5. Section are not recompute.

 

Each time we update the view the section disapear and we need to go in view properties and reactivate section.

 

I also update the assemby file to make sure averything is at ST5.

 

Anyone has input/suggestion or have experience the same thing?

2 REPLIES

Re: Convert ST2 drawing to ST5

Is ST5 patched to the latest Maintenance Patch?

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Convert ST2 drawing to ST5

Hi ken

 

Yes MP11 is install or on its way to be install.

 

After doing few more checks, it seems this was only few drawings.

 

What we figure out, a PMI section was done and apply to the 2D section view. In the process of migrating the check box was removed, when tick again to activate the section things went back.

 

Probably did not fix the problem but at least it was a work around that work.