Reply

Diameter symbol not showing

I am currently using solid edge V20 on windows 7 (64 bit). Whenever I use to place diameter symbol in drafting environment, it shows letter "O". I have also done with automatic dimension but the result remains same. Also tried to change text style but found no result.

 

Can any body help me in this regard...????

9 REPLIES

Betreff: Diameter symbol not showing

Hi,


as far as I can remember, this has to do with a missing font.

 

I suppose the Solid Edge Symbol fonts are missing

 

regards

Wolfgang

 



regards
Wolfgang

Re: Diameter symbol not showing

Could you please shre your screenshot when dimensioning?

 

Is the Diameter Symbol enabled?

 

Yasser

 

Re: Diameter symbol not showing

here u may find the screenshot

Betreff: Diameter symbol not showing

How can I get missing fonts if any...???

Betreff: Diameter symbol not showing

Hi,


could have something to do with MS updates, patches, etc.

 

I remember several cases on different machines, where thos fonts suddenly were away

Copy it back from a valid system and it should work.

 

regards

Wolfgang

 



regards
Wolfgang

Betreff: Diameter symbol not showing

Thanks wolfgang,

 

I have recently switched from XP to win7...
on XP, SE was running perfectly.

 

Can you be more specific about those patches..??
or should reinstalling SE would work..??

Betreff: Diameter symbol not showing

Further, I have checked all other symbols too.. but they too do not show the correct smbol

Betreff: Diameter symbol not showing

Solid Edge fonts can be reinstalled from the install media under the " \Solid Edge\Fonts" folder simply by selecting all the fonts in Windows Explorer and dragging and dropping into the "C:\Windows\Fonts" folder.  If you do not have easy access to the install media PM me and I can send you the fonts.

 

If the Solid Edge fonts are already installed  it could be that whatever font you are using for your dimension style is not suitable for Solid Edge dimensioning e.g. Wingdings.  Check the font used and change it to one of the Solid Edge provided fonts.

Betreff: Diameter symbol not showing

Thanks to all..

 

It works finally...

I just reinstall software and get it back again..

again thanks for your precious opinions/replies...

 

Regards

AM