Reply

Drawing in draft

Hello,

 

I'm reading this forum for quite a while now, and learned alot because of it.

 

But now I got a question myself. Whenever I want to draw a rectangle in a draft it doesn't show me a preview of the rectangle but instead I see a messy red line. After I release the mouse button I get the rectangle just like I wanted. The same thing happens when I want to draw a circle or an arc.

Is this a setting I miss clicked? And if so, where can I find it?

 

I hope I explained myself well.

 

 

 

3 REPLIES

Re: Drawing in draft

That's how it should work. Man Wink

...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user

Re: Drawing in draft

Thank you! I was not aware of the difference between just clicking and holding the LMB.

Re: Drawing in draft

[ Edited ]

FYI....that holding the LMB + drag combo, also works when in some of the other commands, such as trim & trim corner.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10