Reply
Solved! Go to solution

Edge bar not sticking to edge of display

Why is it impossible to "dock" the edgebar to the upper edge of the display on the left of the screen?

 

See attached screenshot

 

Somehow there is an invisible bar of 10 mm of 1/2 " running accross the left half of the upper edge, preventing the edgebar to stick magnetic to the upper edge ?

 

Anyone else with the same problem and hopefully a solution ?

 

Kind Regards,

 

 

Jan Bos

2 REPLIES
Solution
Solution
Accepted by topic author Jan_Bos
‎08-26-2015 04:32 AM

Re: Edge bar not sticking to edge of display

Hi,


try to start any feature function and You will see the SmartRibbonBar just there.

Move it to the right and then the edgebar will be able to be moved up.

 

 

Hope this will work

 

regards

Wolfgang

 



regards
Wolfgang

Re: Edge bar not sticking to edge of display

That is the solution... the smartribbonbar is to far left...

Many thanks Wolfgang..