Reply

Failed on Edit Dimension on Synchronous

Greetings to All Solid Edge masters. Smiley Happy

 

Recently I started using Synchronous on Solid Edge. On this case, I had problem on editing the dimension of diameter (picture shown). Can you guys help me why the dimension won't change? I already tried to turn off all the rules, but it still not working (picture shown). I also attach the Parasolid.

 

Picture 1. Edit Diameter, All Rules ActivePicture 1. Edit Diameter, All Rules Active

 

 

Picture 2. Edit Diameter, Rules Turn OffPicture 2. Edit Diameter, Rules Turn Off

 

 

Picture 3. Failed MessagePicture 3. Failed Message

 

 

Thanks for the helps.

 

Regards,

Thio.

College student.

6 REPLIES

Re: Failed on Edit Dimension on Synchronous

[ Edited ]

I am able to edit the 7.9 dia hole without problems; using ST 8 though.

Can you share the Solid Edge file instead of a Parasolid?

   

~Tushar

Re: Failed on Edit Dimension on Synchronous

ST9 MP2 it is also possible, but we have the parasolid. If you import the parasolid yourself are you able to change the diameter. Else try the hole recognizer and see if you can change the hole after that.

Re: Failed on Edit Dimension on Synchronous

Hi Tushar.

thanks for your response.

I got the file already on Parasolid format, and I change to the Synchronous Sheet Metal, so yes, maybe the problem is on the beginning file.

Re: Failed on Edit Dimension on Synchronous

I am using ST6. but, I dont know the original file is from what type.

 

Thanks.

Re: Failed on Edit Dimension on Synchronous

f the hole recognizer doesn't do the trick, maybe you can try a cut and paste and attacht the hole again

Betreff: Failed on Edit Dimension on Synchronous

HI,



also,

 

 

changing of cylinider diameter is no issue

 



regards
Wolfgang