Reply

Frame name list

Hi Everyone,

Related to frame list on part list.

is there a way to make it automatically as assembly frame list?

frame list on draft only show me the frame type with quantity.

in my assembly view wizard, i have rename every single frame to it's name.

is there an automatic way to generate everything on my part list table with it's own name?

 

Thank you

 

5 REPLIES

Re: Frame name list

Hi,

 

There is no way for this directly. I have to save as your framework and components will get unique names...

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Frame name list

Hi Lmic,

Thanks for your reply.

 

Do you mean i have to save it as neutral format (parasolid,Iges,etc) first then re-open it with solid Edge prior to drawing creation?

 

Thanks & Rgrds

 

Destian

Betreff: Frame name list

Hi,


I think, this also from the point of BOM might not be absolutely correct, since there are several frames which are completely ident.

So there are 4 pieces of the long one, four of the middle once and 4 of the vertical once

 

I don't think that they should be listend as different frame components, should they?

 



regards
Wolfgang

Betreff: Frame name list

Hi Hawcad,

 

Let's ignore my previous example, seems that i have given a wrong example.

 

Please see the following Picture for closely example that i need.

 

 

Is it possible to show renamed frame inside my BOM?

 

Thanks & Rgrds

Betreff: Frame name list

Hi,

 

Solid Edge uses "embedded bodies" when using framework design and it doesn't make "unique" parts from it...

But there is a way, when you can save as frame components. There is a little problem with this, because it will not be direct link between original assembly and "saved as" assembly...

 

Here is a video:

 

 

Yes, you can overwrite BOM's cells, double click on BOM, select a cell and right click and choose "overwrite cell"...

 

BR, 

Imics
http://solidedgest.wordpress.com/