Reply

Half cylinder, but radius shows up as "L"

I was making a print of a pretty simple rolled part that is a half cylinder. When I was dimensioning it, and threw a radius on it, instead of R it shows as L. I've had this happen on parts before, but it was always on parts that had something more complex going on with the rounded area. So I figured it was just a glitch this time, then I go into my part and it displays as L using pmi as well. This is a simple enough part, what the hell is going on with it?

 

I'm attaching the part, though it has IPC's in it and I'm not going to include the other part, sorry I can't.

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
3 REPLIES

Re: Half cylinder, but radius shows up as "L"

I could make it give an R value by forcing it on the dimension ribbon by clicking the radius setting twice. The first click gives you diameter for some reason.

Bruce Shand
ST9 MP3 - Insight - Win10 - K4200

Re: Half cylinder, but radius shows up as "L"

It's because the edge of your Part Copy is not an arc but rather a B-spline curve, thus the dimension defaults to length.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Half cylinder, but radius shows up as "L"

Any idea how this could have happened? What causes things to become a b-spline curve?

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"