Reply

Harness still not useable in ST7

There are two issues that completely prevent us from using the harness module - first, there is no way to make a splice.  We can almost do them with blue-dots, but they don't play will with cables and bundles.

 

Which brings up the bigger issue - bundles don't at all work like they would if someone were actually wiring an assembly and then creating bundles.  For one thing, the limitation that a wire can only be a member of one bundle is an unreasonable limitation.  When we create wire harnesses, we may have 10-12 wires that originate in one area, with 2 or 3 of them running the entire length of the harness, but with others breaking out in multiple branched areas.  A bundle needs to be something that merely collects multiple wires into one routed path.  And one wire may absolutely be a member in more than one bundle.  I've been waiting for a useful harness setup since ST5, and am still waiting.

4 REPLIES

Re: Harness still not useable in ST7

AviatorDave,

I'd be glad to discuss this with you and better understand some of your requirements.  Please email me directly at ronald.conerly@siemens.com.

 

Thanks

Ronnie Conerly

Product Planning

Thanks
Ronnie Conerly
Product Manager, Solid Edge

Re: Harness still not useable in ST7

Ronne, it would be good to share the answer to me also. I have the same challenge & using ST6.

Re: Harness still not useable in ST7

Harness Savvy,
I am getting putting together some documents on harness but they aren't ready yet. Will let you know when they are ready. Thanks
Thanks
Ronnie Conerly
Product Manager, Solid Edge

Re: Harness still not useable in ST7

Thanks for your reply. I am doing a project for my customer. if you share
the document ASAP, it will be great for me.

--
With warm Regards

Vijayan C

"One today is worth two tomorrows."