Reply
Solved! Go to solution

How to increase a frame length in assembly

Dear sir ;

       I need your help. How to increase the frame length in assembly model. if you have any video link please sent't me 

    

4 REPLIES
Solution
Solution
Accepted by topic author sasi
‎08-26-2015 04:32 AM

Re: How to increase a frame length in assembly

The easiest way is to start with a sketch and put the required relationships and dimensions on there.  However if you have already created the frame you can attach dimensions to the individual frame elements.  You can then simply edit these by clicking on them and changing the value.  Alternatively you can define a formula for any of the dimensions to be related to one.  Enter a formula by double clicking on the dimension as shown in this video:

 

http://www.youtube.com/watch?v=cteAKYPTgDc&feature=youtube_gdata

 

Hope that helps,

 

Frank

Edinburgh University

Re: How to increase a frame length in assembly

I think there is even a quicker way...if it still works in ST7. Double click the dimension you want to be driven and then single click on the driving dimension and hit enter. This automatically builds the link you were showing via manual input. Repeat for the other two dimensions and you're done.
--
Ryan Gudorf
CAD/CAM Supervisor
Budde Sheet Metal Works, Inc.
Windows 7 Professional x64 SP1
Solid Edge V20
NX10.0.2.6
TC10.1.5 in Testing
32 GB RAM, nVIDIA Quadro K4200

Re: How to increase a frame length in assembly

You're right, that is quicker and it does still work in ST7.
Edinburgh University

Re: How to increase a frame length in assembly

hi:
Frankmill i am happy very use full for given a solution

Thanks&regard
ANAND.G