Reply

I need to sketch the following metal shhet part

Although it a simple part I didnt success doing it.

Can anyone help me please?

11 REPLIES

Re: I need to sketch the following metal shhet part

My first thought is to use a contour flange. draw the side view as a single line (top or bottom). Then create a contour flange from that line.

 

My other Idea is to create dimples, but that is not nearly as simple.

Re: I need to sketch the following metal shhet part

Contour Flange in Ordered, doesnt like it in Sync. 

ST8 MP11 / ST9 MP02

Re: I need to sketch the following metal shhet part

I have the same idea as Chris - Contour flange in ordered, bu will really wait for Sean and Imics to see if this really turns out to be so simple as it appears Smiley Happy

Re: I need to sketch the following metal shhet part

[ Edited ]

Hi there @Aviad,

 

Just as others have mentioned, easiest way I know to create this form, is by using the "Contour Flange" command.

 

Something like this.... [ST8 ordered file also attached...can also be done in Sync] To speed the example file up, I used a pattern for the multiples, but could just as easily be part of the profile.

 

Node Strip [1].png

 

Node Strip [2].png

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: I need to sketch the following metal shhet part

Hi SeanCresswell,

 

Can you please explain/send a short video which explain how did you create it?

 

Thanks,

Aviad.

Re: I need to sketch the following metal shhet part

[ Edited ]

Hi @Aviad,

 

It really is, just as plain as the geometry you see in my previous screen image.....hope this video helps.

One thing, not so easy to pick up in the video, is the key stroke "A" [for "Arc"], while creating the line segments of the profile. I also omitted placing a line [set to construction] to center the node, and any dimensions.

 

(view in My Videos)

 

If you have ST8, you can interogate the file I attached previously, to see all of what I did......the pattern [may not be how you want to do this] has a few formula driven dimensions on it, and that's pretty much it.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: I need to sketch the following metal shhet part

Hi Sean,



were You succesfull with unbend the patterned contour flange?

I only was able to unbend it (sync and sequ) when only havin one contour flange but not after pattern it.

 

 



regards
Wolfgang

Re: I need to sketch the following metal shhet part

[ Edited ]

Hi Wolfgang,

 

Yes, no problem performing "unbend" & "rebend" of the patterned contour flange. [see updated file]

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: I need to sketch the following metal shhet part

I did exactly what you showed in the video so what am I doing wrong that I am getting this error?

Please see my screenshot.