Reply
Solved! Go to solution

Is there a way to set the default dimension precision in 2D draft

The default precision level for dimensions in 2D draft is set at 4 decimal places. Is there a way to change this?

3 REPLIES
Solution
Solution
Accepted by topic author michele
‎08-26-2015 04:32 AM

There are 2 options to consider when changing unit displa...

There are 2 options to consider when changing unit display in Soldi Edge.

 

File Property Units and Dimension style units.

 

In general:

File Property Units will control the display from system generated or displayed fields

Dimension Styles will controll display of user placed dimensions

 

1.) App button, properties, File Properties, Units and advanced units.

2.) Styles, dimensions, modify (or New) then edit as desired

http://screencast.com/t/JqmpbVwne

HTH

 

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: There are 2 options to consider when changing unit displa...

As Matt said, change your Dimension Style on the Units tab to the desired precision level. You will want to do this to your Draft template so all new Drafts inherit the setting.
Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: There are 2 options to consider when changing unit displa...

Thank you both. The dimension, modify was what I was missing.