Reply

Keyshot - Animation question

Dear all,

I have created a view path in Solid Edge, just a simple rotation in the clockwise direction.

 

After edditing the .bip file in keyshot I want to create a anumation.

Now something happens what I have not selected.

 

I have made the view in perspective, the background colour white and the zoom view so that the item is fully visible in the window.

When I want to preview or play the animation in keyshot the settings mentioned above are all resetted. How do I keep my settings so the animation is correct?

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches
4 REPLIES

Re: Keyshot - Animation question

[ Edited ]

An example of the rendered images that is made so far.

All the setting are resetted.

(view in My Videos)

 

It takes ages for rendering 50 images, so I only have the first 1,53 seconds

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Re: Keyshot - Animation question

Dear all, I think no one knows how it works Smiley Wink

 

What I have found is that the setting for perspective must be done in Solid Edge it self. Other settings like the background seems not be transferred.

 

A small video about what I have done can be seen in Keyshot fun thread.

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Re: Keyshot - Animation question

In Keyshot, the perspective is controlled by lens focal length, more like a camera than a CAD program. I'm not sure if or how SE's perspective distance translates into lens focal length, so you might want to compare initial views of KS with the final views of SE before transition.

Re: Keyshot - Animation question

@MLombard, I know that it works different.

But for some reason when I have no perspective setting in Solid Edge before transmitting to keyshot, keyshot will not display the animation in perspective.

 

It might be a Keyshot problem or a transmitting problem

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches