Reply

Need help to use Silid Edge....

5 REPLIES

Re: Need help to use Silid Edge....

Hi there,

 

What sort of help do you require?.......a few specifics about what exactly you're looking for will go a long way towards getting replies high quality of contributors on this forum, & community.

 

For things like....

  • Computer system selection
  • Installation of Solid Edge
  • Creating first Part, Sheet Metal, and Assembly models
  • Drafting [2D geometry, or from 3D models & assemblies]
  • etc....

What experience do you have with 2D &/or 3D CAD?, or mechanical drafting??

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Need help to use Silid Edge....

I did post a picture but cant see it.

On win 10, when im done with installation of solid edge for academy student. I began with ANSI Part and it said error : Termination Log : An eeror has occurred SE must close. We are sorry for the inconvenience. if the problem is reproducible frequently please open an IR using you customary process . Saving the files to disk may result in a corruption of the date.

 

Re: Need help to use Silid Edge....

Hi there,

 

OK, so a few things come to mind.....

Firstly, probably best if you post your questions to the "Student Edition" specific forum, as there are some small nuances that pertain only to that version.

Second, while it "should" run, the current release of Solid Edge is not certified to run Windows 10, and some errors could be specific to that operating system, that no solutions exist for yet.

Third, can you list your system specs, as it may have incompatible hardware. [there are some system tweaks to reduce the system drain, if required]

 

If you can find it, you might post the "Termination Log" file[s] here for further analysis & feedback.

Look in "C:\Users\user name\AppData\Roaming\Unigraphics Solutions\Solid Edge\Version 107\Log Files"

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Need help to use Silid Edge....

Hi,

 

I've posted this on the Facebook too, that you must install Maintenace Pack 4 (last released) for ST7!

 

It will work! Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Need help to use Silid Edge....

[ Edited ]

@Imics 

 

Problem is even more difficult, as this is the Student Edition, so no "MP's" are available.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10