Reply

Performance Killer "Virus Scanner"

Just some hints about Performance and Virus Scanner.

 

Whenever there is an issue about performance - I know it is always Smiley Happy - we check the Virusscanner Software.

Opening an assembly with Virus Scanner turned on 3 Minutes - turned off less then 40 seconds

 

Here are some hints about it:

  • put the Solid Edge files in the exception list (.asm, .cfg, .psm, . par, .dft)
  • put the Solid Edge application in the exception list
  • for the Insight-Users put the local Cache-Directory in the exception list because there are also other file types than the Solid Edge file types

Important: Check that the Virusscanner has really recognized the new rules

 

Hope this will help to solve some of the performance issues

 

Have a nice weekend

 

Stefan

smitsch@unitec.de
www.all4edge.de