Reply

Query in selection tools for filtering standard parts library

Hello

 

I want to make some  new configuration.

 Configuration where are visible only all standard parts added to assembly from SE standard parts library

 

I want to use to filter this  type of parts using Selection tool-> Create new Query

What should be included in fields of query.

 

 

Regards

 

Marcin

 

 

11 REPLIES

Re: Query in selection tools for filtering standard parts library

Hi Marcin,

query selection depends mostly on part properties.

So I think the easiest way is to define unique property to all standard part (same propety to all standard parts) and then define query with this property.

 

Ota

Re: Query in selection tools for filtering standard parts library

Hello

 

Thanks for help

 

It works

But unfotunately I added a wrong name of custom property to  standard library.

I want remove this custom property from  all standard parts.

How to do this fast? Any method simillar to adding custop property?

Re: Query in selection tools for filtering standard parts library

You're welcome.

 

It is a good question how to delete custom property from multiple parts. I will look into it.

 

Ota

Re: Query in selection tools for filtering standard parts library

I've founded something

 

http://www.eng-tips.com/viewthread.cfm?qid=375951

 

http://barhamsoftware.com/SE_Tools/index.htm

 

I'am trying to use this software but I'am doing something wrong I think or software does not work properly

Re: Query in selection tools for filtering standard parts library

It is possible using automation (macro) but don't know if a program already exists and freely available.

How did you add the wrong property name to multiple parts initially ?

 

Re: Query in selection tools for filtering standard parts library

I added it using Se Standard Parts administrator

Right click on required part or norm and You can add Your own custom property

Re: Query in selection tools for filtering standard parts library

Right so the PropertyRemapper program seems to be the program you need to solve the problem.

Setting the PropertyName="" in the config file will do the trick.

What problem are you facing ? Any error message ?

 

Re: Query in selection tools for filtering standard parts library

Any errors. Everything looks ok.

But property was not deleted

Re: Query in selection tools for filtering standard parts library

Are all files read-write enabled ? 

Some macros and perhaps this one too, are programmed to not show any warning/error but will also not function.