Reply

ST7 MP1: Empthy pdf

I have a dft:

When I save this as a PDF file the drawing nor the dimensions are translated. (see attachment).

 

When my colleague does this with ST7 (no MP) the pdf is correct. Other people with the same problem?

 

...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user
3 REPLIES

Re: ST7 MP1: Empthy pdf

No, just tested this with one of our drawings using ST7 MP1 and it came out just fine.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: ST7 MP1: Empthy pdf

Probably the Solid Edge Velocity PS Printer 2.0 is not installed correctly. Try to reinstall it

Re: ST7 MP1: Empthy pdf

I don't think that's the problem.
Other drawings convert perfect.
Also, this drawing is printed on paper just like the pdf, so without drawing.
...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user