Reply

ST8 - Re-attach DIM via ALT key

In ST7 it was possible to re-attach a dimension to another line or reference via the ALT key.

Now in ST8 it seems that this smart solution is disabled. Is that correct?

 

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches
14 REPLIES

Betreff: ST8 - Re-attach DIM via ALT key

Hi,


no will works here for me as usual

 

regards

Wolfgang

 



regards
Wolfgang

Betreff: ST8 - Re-attach DIM via ALT key

I see 2 points, do you take the point closed to the reference?
-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Betreff: ST8 - Re-attach DIM via ALT key

Hi,

 

 

... the red one!

 

regards

Wolfgang

 



regards
Wolfgang

Betreff: ST8 - Re-attach DIM via ALT key

Weird, I don't see a red one and after many tries it is still impossible.

Thanks anyway
-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Betreff: ST8 - Re-attach DIM via ALT key

I see a gray and a blue dot.

When you press Alt and than select the gray dot you can reattach the dimension.

...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user

Betreff: ST8 - Re-attach DIM via ALT key

I will reinstall SE (again). It is strange that you all can do it and I can't.
-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Re: ST8 - Re-attach DIM via ALT key

Hi,

 

I'm having some problems here too.

 

Still can't find the exact "step to reproduce" so I didn't filled an IR so far.

 

The only thing I find is that it seems to be related, at some point, with "zooming" and/or graphics.

 

Some times, when I can't select the dimension connect handle to re-attach the dimension, I zoom out a little bit and then, it work properly.

 

Some other times, I drag the view out of the working sheet and then I can re-attach the dimension.

 

So, that's why I think it's "zoom", "screen refresh" and/or graphics related.

 

Regards,

 

 

Michel Corriveau

Logiag

ST8 MP01, Win 7 Pro x64 SP1

Re: ST8 - Re-attach DIM via ALT key

I cannot believe that it should be a 'zoom' problem.
-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Re: ST8 - Re-attach DIM via ALT key

I've had some problems reattaching dimensions as well.  The first draft I updated in ST8 had some detatched dimensions and I struggled getting them to reattach.  I tried simply dragging them to the correct geometry and then using the alt key without luck.  A little while later, on another file, everything worked fine.  I'm not sure what is causing the problem. Could it be the new handles for dimensions in ST8?

 

Kyle

Kyle Joiner
IPA LLC
ST9 MP1