Reply

ST8 and Keypoints

Hi

 

In ST8 is it possible for the default setting for keypoint selection to be "ALL" instead of "Centre and End Point?

 

Or have I been missing a setting somewhere to make this the default...?

 

That is all Smiley Happy

 

Thanks


G

5 REPLIES

Re: ST8 and Keypoints

Hi G,

 

Good point.

 

My preference would be for these 3 active: end point, midpoint and center.

A setting in the Options dialog would be best.

Also another setting would be welcome - whether to terminate a command after completion or continue with the last command, so that user doesn't need to press Esc or Select.

 

Just my 0.02 dollars.

 

~Tushar

 

Re: ST8 and Keypoints

Hi,

 

It could be good too, if Solid Edge remembers the last keypoint selection.

 

Yasser

Re: ST8 and Keypoints

@Tushar I would agree with those as the defaults. Midpoint is the one I use the most.

The less amount of mouse clicks the better Smiley Happy

Re: ST8 and Keypoints

ST8? Already a beta release?

-------
Daniël Schuiling
Project Engineer @ EMCÉ Winches

Re: ST8 and Keypoints

Yes. ST8 is in Beta, but most people who are using it can't comment yet.

Jason