Reply

ST9 search for parts using windows indexing failed!

Hi,

can anybody confirm wether this is a software problem or some missing routines I've forgotten to do.

 

I have indexed a small directory structure at local disc with a couple of Solid Edge files

Indxing has been finished (see attached picture ...1305) and has found approx. 1900 files

 

20160824_1305.PNG

So when searching for all files - Filename includes "*" all files might be found and shown.

See for example picture 20162408_1300

 

20160824_1300.PNG

 

If I try a more focused search for docnumber includes "*04*", where I supposed the search bringing up only those files which includes a "04" within the filename the message "Nothing found" appears. (pic. ...1302)

 

20160824_1302.PNG

 

Same if searching for Title "*bush*" which definitefely will be there brings error message (pic. 1301)

 

20160824_1301.PNG

 

So is this a normal behaviour or is that a bug?

 

 

 

 



regards
Wolfgang
2 REPLIES

Re: ST9 search for parts using windows indexing failed!

We discovered also problems in using the new search capabilities.

 

- Search results are not their

- Where used is not working

 

We opened PRs for that so I suggest to wait for the first MP.

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: ST9 search for parts using windows indexing failed!

Hi Stefan,


thanks for the answer, so it is more a Solid Edge issue than a Windows problem?

 

So let's wait for the MP1 and hope that it will be fixed there

 



regards
Wolfgang