Reply

Sheet metal flange 90 degrees sharp edge rather than round radius

We manufacture rigid boxes.  Most material we use are .098" chip board with "V" groove so that when folded to 90 degrees, the outside edge becomes sharp 90 degrees not like sheet metal round radius.  Any suggestions?  Thank you.

2 REPLIES

Re: Sheet metal flange 90 degrees sharp edge rather than round radius

Hi there,

 

See if @Imics video gives you a possible insight into a workable solution.

 

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Sheet metal flange 90 degrees sharp edge rather than round radius

Hi,

 

I hope, this video will be helpful for you:

 

Sorry, dims are in mm not inch, but you can reproduce the steps.

 

BR,

Imics
http://solidedgest.wordpress.com/