Reply

Solid Edge Mold Tooling ST7 pdf file error

Can anyone try to open Solid Edge Mold Tooling ST7.pdf? The one from SE-ST7 DVD does not open, I downloaded the SE ST7 file from the GTAC website, the same error. Both location show 1KB. Can someone tell me where to go and download it or send it attached for me? 

 

Thank You,

Marc

3 REPLIES

Re: Solid Edge Mold Tooling ST7 pdf file error

Hi Marc,

 

No, I see that [file size & error] on the DVD also.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Solid Edge Mold Tooling ST7 pdf file error

Hi,

this document is not the classic PDF (Adobe like). It is some sort of configuration file for installation.

 

I believe that MoldTooling has no PDF documantation available, only help and tutorials in *.chm files, that are available after the MoldTooling is installed.

 

Ota

Re: Solid Edge Mold Tooling ST7 pdf file error

Thank You Ota,

I don't have license for MoldTooling. I just wanted to have a look to see what MoldTooling can do.
Marc