Reply

Solid Edge Round to Square

We need to produce a few pieces of metal from round to sqare.

 

The competition can do that see

 

https://www.youtube.com/watch?v=gtvkfs8UvLk

 

Do we have a command to solve this or..

 

Kind Regards,

 

 

Jan Bos

 

 

 

7 REPLIES

Re: Solid Edge Round to Square

Yeah, you have to use ordered sheet metal for that. Lofted Flange.

Re: Solid Edge Round to Square

Hi Matt,

 

Yes.. lofted.. but this is not producing the bendlines needed form the part.

 

Reg.

 

Jan Bos

Re: Solid Edge Round to Square

I think you could do it with the Bluesurf command.

 

Yasser

Re: Solid Edge Round to Square

Jan,

in the folder /Solid Edge ST8/Training/Sheet Metal/ you find a couple of example parts. E.g "SE_Transition_SR.psm", in where you by changing a couple of parameters can form your version.

 

/Ulf

Siemens EMEA GTAC Support

Re: Solid Edge Round to Square

Hi,

 

Here is an other solution:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Solid Edge Round to Square


Jan_Bos wrote:

Hi Matt,

Yes.. lofted.. but this is not producing the bendlines needed form the part.

 


Hi @Jan_Bos,

 

Go to the Lofted Flange - Options, and on the Bending Method tab, check the box for "Use triangulation......."

 

 

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Solid Edge Round to Square

On what ST version are you working? I have a standard assembly where you can change eveything with variables. Round, Square, Concentric, Excentric you name it.

 

You can only have the bendlines not the angles which some other programs can. My company has this high on there wish list!

 

But this model works great on ST6 but will make SE crash on ST8 something with the change in corner treathment change in ST8. Will be fixed in ST9 (Siemens call 7565775).