Reply

Solid Edge ST6 API - Help with saving four faces of a part to pdf

Hello,

 

I have a .NET program that saves part files as 3d pdfs or as plain pdfs with a default isometric view. This was simple enough, but I was wondering if it is possible to save the bottom, top, left, and right right views to a single page. If not, how would I go about saving each face to its own page in a pdf? I have been scouring the Solid Edge API documentation but figured I should ask for help going about this. If anyone could point me in the right direction I would appreciate it.

 

Thanks

 

1 REPLY

Re: Solid Edge ST6 API - Help with saving four faces of a part to pdf

The right direction is to go to the Solid Edge Developer Forum and post there Smiley Happy

http://community.plm.automation.siemens.com/t5/Solid-Edge-Developer-Community/ct-p/SolidEdgeDevelope...

 

Lots of folks there who would be happy to answer that question.  This forum is the Solid Edge User forum and not many who do API programming hang around here.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1