Reply

Solid Edge ST6 - Maintenance Pack 10 Announcement

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP10) for Solid Edge ST6 is now available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

--- Maintenance Pack Policy --

 

We release Maintenance Packs for CRITICAL items only. Maintenance Packs are available

up to a maximum of 15 months following the release date of the English version. The

release date for Solid Edge ST6 English was 7/19/13, making the Maintenance Pack

cutoff date 10/19/14.

 

--- Office 97-2003 File Types ---

 

Customers have reported problems with SEEC interacting with Office 97-2003 file types.

 

   Example: It not possible to open an excel spreadsheet from the Solid Edge variable table.

 

File open is failing because Microsoft Office 2010 added security checks relating to

opening Office 97-2003 files. Therefore, in order to open Office 97-2003 file types

in this manner the SEEC Cache folder location must be added to the Microsoft Office

application’s Trusted Locations.

 

   Example: Add the SEEC Cache location to:

 

     File->Options->Trust Center->Trusted center settings->Trusted locations

 

================

Download Location:

================

 

ST6 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST6/

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===Assembly===

PR 1885858: Frames is not updated properly when modifying sketch dimensions

PR 1984033: Adjustable part will jump away from its position after updating all links

PR 1991947: A specific part of an assembly is not translated into the resulting step file

PR 2225984: Alternate Assembly preview bitmaps not always being updated on save

PR 7138768: Assembly constraints will not resolve after edits with Large Assembly add-in

PR 7160098: Problems selecting a reference axis after the original is deleted

PR 1994198: Impossible to select component in frame application

PR 1984803: Failed assembly relationships when opening some alternate assembly files

 

===Draft===

1990232: Performance issue in drawing view update

PR 1992068: Prevented copying a view due from one document to another

PR 2236774: Dimension of value '0' is displayed in the draft

PR 7168524: Automatic centerlines were not all being created for an assembly view

PR 7171445: Losing Radial and Diameter symbols during import from DWG

PR 7171484: Angle dim Limit tolerances are incorrect after import from DWG

PR 7171605: Images such as TIF and JPG are not positioned in ACAD

PR 7176666: Most angular PMI dimensions do not display in PMI based DV

1989738: deleting a detailed drawing view leads to a crash

PR 1993512: Grid origin moves when opening previous version file

PR 1994463: Dimensions between Centerlines get wrong scale when doing a Copy/Paste

PR 1995014: Arranged dimension changes after closing the Draw In View mode

 

===Part/Profile/Sheet Metal===

PR 1971089: Suppress/unsuppress of group which contains plane do not work

PR 1978707: After creating revolved cuts a part does not flatten

PR 1991815: Flat Pattern fails, if using DIN.PZL instead of Standard Formula

PR 1991664: 'Discrete list' AND 'Min/max limit' are marked and cause a Syntax Error

PR 7147657: Family of parts EdgeBar display issue

 

===Insight===

PR 7152750: Folder map Dialog should never appear during File Open

PR 1984313: "Free Text" search problem with option "Search for results in subfolders"

 

===Insight Connect===

PR 1990745: Standalone Solid Edge Viewer doesn't open all parts as designed

PR 7142238: Revisions issue with LCA & Revise operations losing revision history

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7179508: Changing the Part container properties on the CPD does not take effect

 

===Solid Edge Embedded Client===

PR 1991572: Problem setting SEEC_ItemTypeList_SE Part and SEEC_ItemTypeList_SE Draft

PR 1992713: Incorrect Item ID when using display names

PR 1993092: BOM mismatch with Save As Copy of read-only Precise IPA'ed assembly structure

PR 7157794: Save Copy As on an item with a drawing, gives a different part number

PR 7164279: File - Open of read-only (migrated from TcE) Part file displays strange error

PR 7167956: Save Copy As creates undesired link between new Draft file and original Assembly

PR 7168059: Open as read-only setting uses stale data.

PR 7168465: MT9_Drawing item type naming rule patterns for ID and revision are ignored

PR 7169854: Item Name in Solid Edge CPD not synchronizing between Part and Draft file

PR 7170830: Insert Part Copy behaves differently in Solid Edge managed vs. unmanaged

PR 7174855: Save As of migrated data changes the Item Name on the CPD from original

PR 7175353: Remove All on the Project ID will not remove the Project ID for model and draft

PR 7176006: The Insert Weldment link is shown as a red question mark

PR 1992719: SESE not using Naming Rules on Item Id and Item Name correctly

PR 7181609: Preview Image on Cache Assistant dialog is distorted as width is increased

 

Regards,
Fred White
Siemens PLM Software