Reply

Solid Edge ST6 - Maintenance Pack 11 Announcement

November 20, 2014

 

 

Dear Solid Edge Customer:

 

The latest Maintenance Pack (MP11) for Solid Edge ST6 is now available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

--- Maintenance Pack Policy --

 

We release Maintenance Packs for CRITICAL items only. Maintenance Packs are available

up to a maximum of 15 months following the release date of the English version. The

release date for Solid Edge ST6 English was 7/19/13, making the Maintenance Pack

cutoff date 10/19/14.

 

--- Office 97-2003 File Types ---

 

Customers have reported problems with SEEC interacting with Office 97-2003 file types.

 

   Example: It not possible to open an excel spreadsheet from the Solid Edge variable table.

 

File open is failing because Microsoft Office 2010 added security checks relating to

opening Office 97-2003 files. Therefore, in order to open Office 97-2003 file types

in this manner the SEEC Cache folder location must be added to the Microsoft Office

application’s Trusted Locations.

 

   Example: Add the SEEC Cache location to:

 

      File->Options->Trust Center->Trusted center settings->Trusted locations

 

================

Download Location:

================

 

ST6 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST6/ 

 

==========

Installation:

==========

 

After downloading the Maintenance Pack to your machine, unbundle the zip file and then

dbl click on exe to install the Maintenance Pack.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

Or send an e-mail message (message and subject line should be blank) to: sfbmail-subscribe.plm@siemens.com

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 1997369: No lines in DXF file when using the API Method .SaveAsFlatDXFEx()

PR 1991583: QueryByName doesn't return a result for the "Default" Attribute Set

 

===Assembly===

PR 1994134: When hovering over a Sketch with Connect relationship key points are not visible

PR 1995269: crash when applying certain display configuration

PR 7189285: fence selection performance issue with Steering Wheel enabled in large assemblies using Part Priority mode

PR 7164670: Cutout profiles not placed correctly in some cases with System Library

PR 1994706: SePvAdp.exe doesn't create a JT file from an assembly and exit with error

PR 1997910: new assembly relationships being created when editing an existing relationship

PR 1999083: axial align geometry not displaying properly with inactive parts when selected in the Pathfinder

PR 1129886: Fixed an abort in the assemble command

PR 7164279: Users are prevented from Edit opening Part/Sheet Metal files that are modified in memory

PR 7207561: Mass value in parent assembly is incorrect

PR 7173522: Not getting assembly mass based on user-defined quantity for nongraphic part

 

===Draft===

PR 1986615: Cannot delete link from draft file

PR 1996610: Dimension Style with ',' will not be exported to DXF

PR 7194191: The alignment shape does not move to a new sheet

PR 1128251: duplicate dimensions in a lot of drafts

PR 1997964: symmetric diameter detached if centerline is edited and view repositioned

PR 2247261: Parallel dimensions are abnormal

PR 7196026: abort getting physical properties in some cases

PR 7201475: Crash due to accessing a Null pointer

PR 2248233: The placement of dimensions changes

PR 7218956: Solid Edge crashes after using extend command

PR 1921943: locked dimension changes value when geometry dragged

PR 1986693: Item count balloons that don't have a parts list are not updating.

PR 2250765: Dimensions move when I open dft in ST6

PR 7218956: Solid Edge crashes after using extend command

PR 8252911: SE hangs when zooming and panning

 

===Part/Profile/Sheet Metal===

PR 1977497: property text not solved in this draft

PR 7188619: Material Table Editor not working with Excel 2013

PR 1129164: Crash when saving a Part file, where a feature is pasted in

PR 1973206: Split Body causes the bodies to rearrange

PR 8250101: can't copy sync sketch

PR 2248871: non-reproducible abort during file close

PR 1128844: NX9 part can't be loaded and saved to ST6

PR 1995423: Connect relation to peer geometry does not work by mouse click. The click should now connect the relation. Note: Due to numerous changes in ST7 and not all could be ported back to ST6. Therefore, the line highlighted will not remain highlighted.

 

===Insight===

PR 1990496: Edit Profile (Upload) pops up since ST5MP11 even the part haven't been changed

PR 1985438: File not found message when SE tries to open a renamed FOA, RevMan open OK

 

===Insight Connect===

PR 1959588: RevMan Copy of a Divide Part Master.par + both divided parts = wrong Insight link

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7182587: 'Part.Title' property is not updated in this workflow

 

===Solid Edge Embedded Client===

PR 7189106: Save as fails for this specific Teamcenter Item revision

PR 1991419: Different LOV displayed in Solid Edge compared to Teamcenter

PR 1127691: ST6 removes TC-Absolute-Occurrence Information during upload/check-in

PR 7210424: Assembly Save As does not honor revision naming rule if Item ID is changed first

PR 1128098: Poor performances when creating, saving, or revising a document

PR 7155782: Save As fails when Insert Part Copy used with TC10.1

PR 8250856: Sequence No. synchronization issue when moving from ST2 to ST6

 

 

Regards,
Fred White
Siemens PLM Software