Reply

Solid Edge ST7 - Maintenance Pack 2 Announcement

November 10, 2014

 

 

Dear Solid Edge Customer:

 

Solid Edge ST7 Maintenance Pack 2 for Solid Edge is available for download.

 

Sincerely,

The Solid Edge Team

 

 

============

Release Notes:

============

 

Maintenance Packs are released for CRITICAL items only. Maintenance Packs are available up to a maximum

of 15 months following the release date of the English version. The release date for Solid Edge ST7 English was

08/08/14, making the Maintenance Pack cutoff date 11/08/15.

 

================

Download Location:

================

 

ST7 Maintenance Packs can be downloaded from:

 

   https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/

 

==========

Installation:

==========

 

There were Solid Edge Embedded Client policy file updates in MP2. It’s vitally important that you install SEEC

Administrator, which delivers the policy files to TC_DATA.

 

Maintenance Pack Executables (.exe files) patch existing product dlls. Maintenance Pack executables

are all inclusive and can be installed on top of a base release or any released Maintenance Pack.

 

Maintenance Pack Installs (.zip files) are complete product setups. Therefore, existing versions must be

uninstalled using Add/Remove Programs from the Control Panel prior to installing the new setup.

 

===============

E-mail Notification:

===============

 

To receive direct e-mail notification for new Solid Edge Update or Maintenance Packs, subscribe

to the SFBmail notification.

 

To initiate your subscription, navigate to: http://support.industrysoftware.automation.siemens.com/general/email.shtml for the web interface.

 

=========================================

This Maintenance Pack addresses the following PRs:

=========================================

 

===API===

PR 1997747: Solid Edge crashes with our add-in if a drawing has balloons

PR 1128963: Custom add-in command is removed from Quick Access Toolbar when Solid Edge is restarted

PR 1991583: QueryByName doesn't return a result for the "Default" Attribute Set

PR 1999928: API RevManager LinkedDocuments changed behavior in ST7

PR 1997369: No lines in DXF file when using the API Method .SaveAsFlatDXFEx()

PR 1998444: Abort trying to get access to material Table via API

PR 1994706: SePvAdp.exe doesn't create a jt-file from an assembly and exit with error

PR 7224772: Old material library APIs do not work for a single material library

PR 7216470: Add a property to not resolve links for SEReader

PR 7214771: SEReader reporting original filenames after a rename

Note: The new SEReader.dll and map files are posted on the GTAC FTP server:

                https://download.industrysoftware.automation.siemens.com/solid_edge/ST7/Maintenance_Packs/MP02/

 

===Assembly===

PR 1995269: Crash when applying certain display configuration

PR 7187357: Can’t edit pattern part with surface in assembly

PR 7197155: Incorrect dynamic preview for assembly angular relationships

PR 1998326: KeyShot should be inactive with a Foundation license

PR 7164670: Cutout profiles not placed correctly in some cases with System Library.

PR 1998237: Applying a symmetric bearing load on a symmetric part does not give the expected symmetric result

PR 1909919: Replace Part with Copy gives wrong result when this part have been mirrored

PR 7164279: Open of a read-only Part file displays strange error

PR 7188566: Frames do not render correctly in KeyShot

PR 1995644: Deletion of the category IS using the Standard Parts Administrator also deletes the ISO category

PR 7207561: Mass value in parent assembly is incorrect

PR 8250204: Systems Library doesn't recognize associative Feature in ST7

PR 7173522: Not getting assembly mass based on user-defined quantity for nongraphic part

PR 7216497: insert part copy of asm file with protrusion does not show the protrusion

PR 7217470: Unable to create a part in place. Template not found with Custom list.

PR 8251592: Save as translated breaking links to tubes

 

===Draft===

PR 1997706: Can't locate elements of different type to connect to

PR 7196026: Abort getting physical properties in some cases

PR 1128251: Duplicate dimensions in a lot of drafts

PR 2247261: Parallel dimensions are abnormal

PR 1999206: Can't specify a Parts list through a Display Configuration view anymore

PR 1999705: Parts List will not allow user defined rows to be added

PR 7201475: Solid Edge crashed when performing retrieve dimensions from dft

PR 2248233:The placement of dimensions changes

PR 7212537:Edit list changes when Solid Edge Options are modified

PR 1921943: locked dimension changes value when geometry dragged

               

===Part/Profile/Sheet Metal===

PR 1127865: KeyShot 5 is not running with a Solid Edge Classic borrowed license

PR 1997489: Flat Pattern does no longer work in ST7 but was OK in ST6, regression

PR 1127777: Adding custom property of 'Text' type to a material causes crash/doesn't work

PR 1973206: Split Body causes the bodies to rearrange

PR 1997728: Wrong material , when using create Part in Place

PR 2247477: Code change made due to investigation of SE Crashlog

PR 2249018: FOP master file has lost FOP Tab.

PR 7219732: Cannot create a sweep from a 3D sketch

PR 2248871: non-reproducible abort during file close

PR 7177036: Export JT from SE with Model view is defined incorrectly

PR 7219285: ST7 Distance command doesn't find center points

PR 7196340: Fixed a problem with Filename being truncated when translating to DWG

 

===Insight===

PR 1990496: Edit Profile (Upload) pops up since ST5MP11 even the part haven't been changed

PR 1985438: File not found message when SE tries to open a renamed FOA, RevMan open OK

PR 8250895: Revision Manager crash when opening files from Insight DocLibs

 

===Insight Connect===

PR 7206624: Labels missing for some commands when localized

PR 2248073 : It is impossible to do a "Replace Part with Standard Part" in an Insight Managed

 

===Solid Edge SP, Server, Standalone Client, Solid Edge Client===

PR 7166961: Add to Library is putting files in wrong location

PR 1996701: Part Title not mapped to Item Title

PR 1128234: Element.Titel (Item.Title) and Teil.Titel (Part.Title) not correct

PR 7199708: Delay observed in loading toolbars for drawing with no write access

 

===Solid Edge Embedded Client===

PR 7188611: places linked drawing in wrong location in BOM

PR 7195451: Save As on Assembly assigns Draft to unique Item ID

PR 1991419: Different LOV displayed in Solid Edge compared to Teamcenter

PR 1129164: SE Crashes, when saving a Part file, where a feature is pasted in

PR 8250101: can't copy sync sketch

PR 1128098: Poor performances when creating, saving, or revising a document

PR 1998410: Column "Project ID" disappears, if SEEC is working with SSO/TcCS

PR 7155782: Save As fails when Insert Part Copy used with TC10.1

PR 7225135: Revise creates wrong dataset name when specific custom property exists

PR 7222814: Save As on Draft creates link to original Part instead of new Part

Regards,
Fred White
Siemens PLM Software