Reply
Solved! Go to solution

Weird cutting plane (draft) problem

Hi,

 

I need to place a cutting edge (for a section view), 25 mm. from the end of my part, but Solid Edge change the dimensions to 50% of the correct value.

 

See video:

 

I can probably just type "12,5" in the example video above, but that just feels wrong - to type a false value.

4 REPLIES

Re: Weird cutting plane (draft) problem

It seems, that the cutting plane calculates its position in function of your actual scale 1:2

 

Yasser

Re: Weird cutting plane (draft) problem

[ Edited ]

What's the scale of the view? With sections Edge uses the sheet dimension, not model dimensions in these cases. So it multiplies the dimension by view scale. You can easily see this by changing the view scale then editing the section line. The dimension you place and gets recalculated is the correct dimension in terms of the model at its scale.

Bruce Shand
ST9 MP3 - Insight - Win10 - K4200
Solution
Solution
Accepted by topic author Kenneth
‎09-30-2015 04:41 AM

Re: Weird cutting plane (draft) problem

Hi there,

 

If you need an exacting location for section lines, I normally just use relationships when drawing the cutting plane profile, but have also used sketch geometry placed within "Draw In View", then locating the cutting plane profile to match that sketch, with relationships as needed.

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: Weird cutting plane (draft) problem

The relationship idea was great, worked perfectly Smiley Happy