Reply

When creating a tube how can you split the part so it then can become flattened?

Hi All,

 

Im new to solid edge. Trying to self learn.

 

Ive created a tube and need to flatten so it can be rolled. Am i right in saying that the tube requires splitting before it can be rolled? If so how do i split the tube?

 

Many Thanks,

 

Darren

6 REPLIES

Re: When creating a tube how can you split the part so it then can become flattened?

When I need something like this, I draw an arc. Nearly closed in sheet metal:

This tube can be flattend.

 

...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user

Re: When creating a tube how can you split the part so it then can become flattened?

[ Edited ]

Hi Darren,

 

Further to normal [just as I would do this] solution offered by Joris, and because there is usually at least a couple of ways to accomplish tasks in Solid Edge, you could also draw a pizza segment [obviously, you'd need to dimension accordingly, to have a smaller gap than I have used for illustration] to one end, and use it as a cutout to the full length of the tube, then switch to "Ordered" mode > run "Convert to Sheet Metal" > "Flatten".  Done!

 

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: When creating a tube how can you split the part so it then can become flattened?

Remember that synchronous sheet metal parts must start with a tab, that means they must have a flat area. So a round tube can only be done in ordered.

Re: When creating a tube how can you split the part so it then can become flattened?

Thanks guys still having a couple of problems. Ive got my tube (3mm wall thickness) and cut out a 0.1mm pizza shape all the way through. Then switched over to sheet metal to flatten and this problem occurs. Please see image below.

Re: When creating a tube how can you split the part so it then can become flattened?

[ Edited ]

First of all, start in sheet metal, a sheet metal part is drawn in the sheet metal environment.

Than, the easiest way is draw a nearly closed arc when creating a "Contour Flange".

 

In my prior screenshot you can see all the steps I think.

...........................................................................................................
Solid Edge ST9 & AutoCAD 2017 user

Re: When creating a tube how can you split the part so it then can become flattened?

Champion. Ive cracked it! Thanks