Reply
Solved! Go to solution

Will ST8 run on Windows 10?

Hi

 

Does anyone (Siemens) know whether ST 8 will run under windows 10? Microsoft are offering free upgrades for a year, but that is only of use if ST8 will run on it. The release notes don't mention Windows10, so some clarification would be good.

 

Thanks

5 REPLIES

Re: Will ST8 run on Windows 10?

[ Edited ]

Hi Alan,

 

Check this thread on it....by @Stefan_Mitsch 

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10
Solution
Solution
Accepted by topic author Alan
‎08-26-2015 04:32 AM

Re: Will ST8 run on Windows 10?

ST8 is not supported on Windows 10 because Windows 10 is not a released product, and thus is still a moving target to support.  When it is released, look for a maintenance patch for ST8 to support Windows 10.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Will ST8 run on Windows 10?

Dear Friend ,

Solid Edge ST8 works fine in windows 10 , I am running ST8 on windows 10

Re: Will ST8 run on Windows 10?

"Working" and "supported" are 2 different things.  If you encounter an issue where ST8 doesn't completely work on Windows 10, it will not be fixed if it is not supported.

 

Now Siemens is expecting to support ST8 on Windows 10 with a maintenance patch, however the initially released version is not supported on Windows 10.  Also, some folks have stated that ST7 with maintenance patch 4 (I believe) works on Windows 10, however it will never be supported on Windows 10, and no one can be certain that it works 100%.

Ken Grundey
Production: ST6 MP14
Testing: ST9 MP1

Re: Will ST8 run on Windows 10?

I have been running ST8 on a new notebook since early November. Although I only use it on an occassional basis, it runs fine and I have never had any issues with Solid Edge running.