Reply

Wrong tab appears for file name after opening subassembly

Here's another one:

 

I'm in a main assembly and then open a subassembly.  When I return, the file tab is now showing the name of the subassembly instead of the main assembly.  The tab on the left should say SE-11008 Assembly, Door Bar.  Here's a screen shot:

 

Tab - wrong name.JPG

 

I'm running ST9 MP1

 

Kyle

Kyle Joiner
IPA LLC
ST9 MP1
2 REPLIES

Re: Wrong tab appears for file name after opening subassembly

I believe this may have been fixed in MP2. Try installing that and see if the problem still exists.

 

PR 7792385: Tabs incorrect if Assembly, Subassembly opened and Part in edit mode

Re: Wrong tab appears for file name after opening subassembly

I'll give it a try.

 

Kyle

Kyle Joiner
IPA LLC
ST9 MP1