Reply
Solved! Go to solution

"Undo Cache"? Can I increase the number?

Hey.  I'm looking for something like an "undo cache".  Sometimes my document is unable to "undo" and I haven't even saved.  Automatic saving isn't enabled, so that's not it.  I'm thinking the operation was too big to go back?  I'd like to be able to increase the cache size so I can go back on bigger operations.

Thanks.

6 REPLIES

Re: "Undo Cache"? Can I increase the number?

SE calls it "Undo Steps"

- Application button

- Solidedge Options

- General Tab

     - "Undo Steps" at the top

 

Re: "Undo Cache"? Can I increase the number?

My number of "undo steps" was set to 500.  That doesn't seem to be the problem.  I wonder if there is a "maximum undo filesize"...

Re: "Undo Cache"? Can I increase the number?

I've had the "Undo Problem" before on certain versions....most likely ST1-ST4. Other than the "Undo Steps"....I dont know....

Re: "Undo Cache"? Can I increase the number?

Hmm.  OK.  I'm on ST7, but still a problem.

Solution
Solution
Accepted by topic author Kuli24
‎08-26-2015 04:32 AM

Re: "Undo Cache"? Can I increase the number?

certian opperation force a write to disc.  once thsi happens  undo is reset...

 

Re: "Undo Cache"? Can I increase the number?

Thanks for this.  Man, it seems Solid Edge still has many limitations.