Showing results for 
Search instead for 
Do you mean 

Create Line with Existing Geometry

by Siemens Experimenter Siemens Experimenter on ‎03-13-2013 01:33 PM - edited on ‎12-02-2013 07:24 PM by Community Manager Community Manager (4,756 Views)

Question

How can I create a line in a sketch from existing geometry, like a protrusion or another sketch?

Answer

In the Home tab on the ribbon, inside the Draw group you should see an icon that looks like a white piece of paper with a line under it, that is the Project to Sketch Tool.  You can click the edge of a protrusion or a line from another sketch and project that line on to the sketch you're currently in.