Cancel
Showing results for 
Search instead for 
Did you mean: 

Combustion chamber of CFM model didn't burn

Experimenter
Experimenter

Hi, I'm using the IFP library to build a model of Turbocharged CNG Gasoline Engine. But currently i've found that after i added the turbo group , the CFM combustion chamber didn't burn. All the parameters i've set seem normal . Are there other parameters that can effect the combustion deeply?

1 REPLY

Re: Combustion chamber of CFM model didn't burn

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

Adding a turbocharger should not change the combustion phasing. It will increase the intake mass flow rate and so, increase the volumetric efficiency. In the CFM combustion chambers, the turbulence maps (cut-off/tumble) are function of the volumetric efficiency.

I recommend to:

- check if the volumetric efficiency is correct,

- check if your turbulence maps are defined for those values (if not, a linear extrapoaltion is done and can lead to inconsistent values)

 

Cordially,

 

Thomas