Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I make an HR cross pipe model?

Pioneer
Pioneer

I want to make some model using Hydraulic Resistance library

This model consists of cross pipe

But, I can't find any cross pipe component in Hydraulic Resistance library.

 

 

01.png

 


How can I make an HR cross pipe model?

Could I use two T-junction model instead of one cross pipe model?

 

 

 

p.s. Thanks In Advance

4 REPLIES

Re: How can I make an HR cross pipe model?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Kuro,

 

yes you can use two Tee junctions and a central pipe, something like this picture:

cross pipe in Amesimcross pipe in Amesim

 

Re: How can I make an HR cross pipe model?

Pioneer
Pioneer

  

Hi! Emmanuel_D

 

thank you for your reply

 

so, you mean, cross pipe can modeling in this way?

 

 

03.png

Re: How can I make an HR cross pipe model?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Kuro,

 

ah....  I was a bit too quick with my intrerpreation of a cross pipe ^^

Indeed there is no submodel of such a junction with pressure losses.

 

For this, I would start with a simple/ideal 4-port node from the hydraumlic library and compare it with other alternatives such as chaining Tee junctions. For my simple test-case the differences in flow rate could be considered acceptable - your call!

Though I have to say I don't like the succession of Tee junctions as it's not symmetrical and will depend on flow direction. Another option could be to consider a central volume and four fixed discrete losses at each port.

Flow rate comparison in each branch for each configurationFlow rate comparison in each branch for each configuration

Re: How can I make an HR cross pipe model?

Pioneer
Pioneer

I like the third method.

 

Thanks for the tip Smiley Happy