Cancel
Showing results for 
Search instead for 
Did you mean: 

Submodel for smoothing the signal

Creator
Creator

Hi there,

I'm working with the signal and control-library.
My program calculates but I have a problem with an oscillating signal. Due to that my calculation is really slow in the area of the oscillating signal and I can't implement greaterthan- or lessthan-submodels there because then the calculation fails.

Is there a possibility to smooth the signal with another submodel in an easy way?

You can see attached the 4 oscillating areas.

 

Many thanks in advance!!

6 REPLIES

Re: Submodel for smoothing the signal

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Trompeterich,

 

Maybe you could try to stick a first (or second) order lag after your sensor to smooth out the oscillations.

Like this:

Amesim_smooth.jpg

 

To start with, for the first order lag, use 1e-3 seconds, check input and output signals from the block see if it is satisfactory.

 

Re: Submodel for smoothing the signal

Siemens Genius Siemens Genius
Siemens Genius

If your input signal comes from a table, you could use the filter capabilities of the table editor (Tools > Butterworth filter).

 

If this is computed from your system you could use a transfer function to compute also a Buterworth filter (see https://en.wikipedia.org/wiki/Butterworth_filter#Transfer_function ). But you should also check if this high oscilations are normal, perhaps you did not model enough friction in your model?

Re: Submodel for smoothing the signal

Creator
Creator

Thank you for your fast reply!
But unfortunately the signal has become worse when I implement the first or second order lag...

Re: Submodel for smoothing the signal

Creator
Creator

I don't have any friction in my model...
Should I?
And where?

Re: Submodel for smoothing the signal

Siemens Phenom Siemens Phenom
Siemens Phenom

Without the model and further info about the source of the issue it could be a guess game...

Did you have a look at Help/Amesim demo help or get to start from a running template?

Amesim_demo_tr.png

Re: Submodel for smoothing the signal

Creator
Creator

Thank you for your answers,

I fixed my problems with a discrete delay instead of a continous delay.

With that the oscillations disappeared