Cancel
Showing results for 
Search instead for 
Did you mean: 

Switch between different AMESim versions

Valued Contributor
Valued Contributor

Hello,

I am starting having requests from customer with differents versions of AMESim (14/15)

We have "newly" installed V14, and now we have a request on V15.

I thought I could switch easily between versions, but I tried to open V13 for instance, and became error (from Windows, not AMESim)

Question: do I need a special tool for switching between different AMESim versions? I know there is (was) AMEVer tool

Thanks for any informations

Maxime

8 REPLIES

Re: Switch between different AMESim versions

Experimenter
Experimenter

Hello,

 

It works, if you change environmental variable path in windows system.

 

system variable --> C:\Program Files (x86)\LMS\LMS Imagine.Lab\v1500\Amesim

 

 

 

 

 

Re: Switch between different AMESim versions

Siemens Genius Siemens Genius
Siemens Genius

Hi @mAx,

 

what kind of error do you get?

 

Kind regards

Re: Switch between different AMESim versions

Valued Contributor
Valued Contributor

Hello @Domi

As I said it is a windows issue (I think)

"AMESim.exe has stopped working"Capture.JPG

 

Re: Switch between different AMESim versions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi mAx,

 

in $AME/misc you will find a RunAMESimTemplate.bat which should allow you to run specific Amesim versions.

You need to edit that bat file to specify the path of the current version.

Amesim_bat_file.jpg

 

If that still fails, please use GTAC to raise an Incident Report.

If that works, you can copy a shortcut to this bat file on your Desktop and rename it to "Amesim xx"

 

Re: Switch between different AMESim versions

Valued Contributor
Valued Contributor

Thanks @Emmanuel_D

It works!

Maxime

Re: Switch between different AMESim versions

Experimenter
Experimenter

hi guys,

 

Thank you for your solution .

i Have a big answer, is not possible to run Amesim 13.2 and Amesim 14.2 without modifying every time the system variable AME= ?

 

I have a client where are installed the versions 13.2 and 14.2 but if i give to $AME=Amesim1320 when i want to start 14.2 i receive the windows error and also it applies the other way

 

thank you

Re: Switch between different AMESim versions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Daniel95,

 

here's what you can do:

- you modify the bat file located in each Amesim installation folder as described in my previous post

- you create a shortcut to these modifed bat files on your Desktop, rename the link, modify the "Start in" location and change its icon to make it look niceSmiley Happy

- you can do that for as many Amesim versions as you like

Amesim_shortcuts.png

 

 

 

Amesim_shortcuts_cosmetic.png

Re: Switch between different AMESim versions

Experimenter
Experimenter

Thank You.

I will try but i don't know if it will work because our Standard Users doesn't have admin permission on pc.

I'll let you know.